UL-SCH |
||
---|---|---|
1. General Settings |
2. Transmission Settings |
3. PUSCH Configuration Dedicated |
|
||
|
||
|
||
|
UCI |
---|
1. General Settings |
Displays the identifying number of the selected channel.
Displays the name of the selected channel.
UCI = Uplink Control Information
UL-SCH = Uplink Shared Channel
Choice: Off | On
Default: Off
Double-click or use the drop-down menu to turn the selected channel off or on.
Range: -60 to 20 dB
Default: 0.000 dB
Enter a power level in dB for the selected channel. See Output Power Calculation (Uplink) for a description of how the software applies your power setting.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn scrambling for the physical channel on or off.
This parameter applies only to UL-SCH channels.
Use the Data Source Selection dialog box to select , , or to use for the data.
Choice: None | Every Subframe
Default: None
Sets the data reset method for UL-SCH.
the transport data is continuously repeated seed data which is specified by Data parameter. The transport data is not reset till end of the waveform.
the transport data is reset at the start of each subframe.
This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U01 or greater is valid. Refer to Licenses for more information.
This parameter applies only to UCI channels.
Select a resource block assignment for the UCI from the drop-down list. Your selection is applied to the UCI in the first slot of each subframe. The UCI in the second slot of each subframe is adjusted accordingly. Your setting is displayed in the resource mapping graph at the bottom of the Channel Setup window.
Choice: Off | On
Default: On
This parameter applies only to UL-SCH channels.
Double-click or use the drop-down menu to turn coding for the selected channel off or on.
Range: 8 (ttiBundling = Off
Default: 8
This parameter applies only to UL-SCH channels.
The value is read only. It is the number of available hybrid automatic repeat request (HARQ) processes and defines the interval (number of subframes) between retransmissions. Use the Assigned Processes parameter to enable HARQ processes.
Your setting is displayed in the UL-SCH Tx sequence window (see Transmission Configuration).
Range: 0 to (number defined in Number of HARQ Processes)
Default: 0-7
This parameter applies only to UL-SCH channels.
Enter the numbers of individual HARQ processes, separated by commas (for example, Number of HARQ Processes cell.
) or a range of HARQ processes ( for example, ) to enable specific HARQ processes. The number of available HARQ processes is defined in theYour setting is displayed in the UL-SCH Tx sequence window (see Transmission Configuration).
Choice: Auto | Manual
Default: Auto
Double-click or use the drop-down menu to set the RV Index Configuration.
If
is set to , then the parameter is active. If the parameter in the UL-SCH Tx sequence window is set to , then the next RV Index in the is used for the RV Index of the UL-SCH transmission in the same subframe.If
is set to , then the parameter is inactive. In this case, you can set RV Index for each UL-SCH transmission.Range of sequence length: 1 to 16
Range of each value: 0 to 3
Default: 0, 2, 3, 1
Enter the numbers of individual RV Index Sequence, separated by commas (for example, 1,2,3).
If
is set to , then the parameter is active. Otherwise it is read only. If the parameter in the UL-SCH Tx sequence window is set to , then the next RV Index in the is used for the RV Index of the UL-SCH transmission in the same subframe.Select an uplink channel, then click the
button in this cell to open the UL-SCH
Tx sequence window, or the UCI
Tx sequence window.
Range: 10 ms to Waveform Generation Length, Max 160 ms
Default: 40 ms
Set the length of transmission configuration. The definition of transmission configuration of SCH and related UCI will be repeated to the end of the Waveform Generation Length.
If the Waveform Generation Length parameter is set less than the Transmission Configuration Length, the value of Transmission Configuration Length is changed to be ≤Waveform Generation Length. In summary, the relation between Transmission Configuration Length and Waveform Generation Length is that the Transmission Configuration Length ≤Waveform Generation Length. Refer to the Waveform Generation Length parameter.
|
Channel |
Transmission Configuration Length |
Default Value |
---|---|---|---|
Uplink |
UL-SCH |
The value is available to set 1 -16 Frames With following rule: Transmission Configuration Length ≤Waveform Generation Length |
10 ms |
|
UCI |
The value is automatically set to same value corresponding UL-SCH. |
Same as UL-SCH |
Example: Where the Transmission Configuration Length is set to 20 ms (2 frames), Frames #0 and #1 configurations (Sequences #1 through #20) will be repeated while generating SCH.
Range: 0 to 14
Default:
Enter a value for the HARQ-ACK Offset Index. The table below shows the relationship between the HARQ-ACK offset value and the
|
|
---|---|
0 |
2.000 |
1 |
2.500 |
2 |
3.125 |
3 |
4.000 |
4 |
5.000 |
5 |
6.250 |
6 |
8.000 |
7 |
10.000 |
8 |
12.625 |
9 |
15.875 |
10 |
20.000 |
11 |
31.000 |
12 |
50.000 |
13 |
80.000 |
14 |
126.000 |
15 |
reserved |
Range: 0 to 12
Default: 0
Enter a value for the RI Offset Index. The table below shows the relationship between the RI offset value and the
|
|
---|---|
0 |
1.250 |
1 |
1.625 |
2 |
2.000 |
3 |
2.500 |
4 |
3.125 |
5 |
4.000 |
6 |
5.000 |
7 |
6.250 |
8 |
8.000 |
9 |
10.000 |
10 |
12.625 |
11 |
15.875 |
12 |
20.000 |
13 |
reserved |
14 |
reserved |
15 |
reserved |
Range: 2 to 15
Default: 2
Enter a value for the CQI Offset Index. The table below shows the relationship between the CQI offset value and the
|
|
---|---|
0 |
reserved |
1 |
reserved |
2 |
1.125 |
3 |
1.250 |
4 |
1.375 |
5 |
1.625 |
6 |
1.750 |
7 |
2.000 |
8 |
2.250 |
9 |
2.500 |
10 |
2.875 |
11 |
3.125 |
12 |
3.500 |
13 |
4.000 |
14 |
5.000 |
15 |
6.250 |